Hi Team,
Here we are trying to configure AD9576 eval board. We need your support in configuring the SPI communication ( Pins in Eval board hardware and the setting to be used in ACE installer).
Also can you please assist in,
1. To convert the on-board crystal Ref input 25MHz (fractional-N translations Input) to 16.369MHz output frequency with Dual PLL lock, and the required registers values to be configured for
the same using Eval board ACE installer.
2. To convert external Ref input 10MHz (fractional-N translations Input) to 16.369MHz output frequency with Dual PLL lock, and the required registers values to be configured for the
same using Eval board ACE installer.