Post Go back to editing

Not output clock

Thread Summary

The user is troubleshooting an issue with the AD9246(DPLL) not outputting clocks on a custom board, despite APLL and DPLL being locked. The final answer suggests enabling auto-sync mode in the ACE tool for both DPLLs and setting jumpers P300-P304 between pins 2 and 3, connecting TP307 to TP308. The user has also provided the ACE configuration file for further review.
AI Generated Content
Category: Hardware
Product Number: AD9246

We are currently evaluating the hardware.
We are having trouble with ANALOGDEVICES AD9246(DPLL) not outputting.

We are using the ACE tool to set the register settings, but it does not output.
Could you please tell me how to check the cause of the no output.

Parents
  • We have attached the ACE configuration below.


    We have configured the registers on the custom board and confirmed that the APLL and DPLL are locked.
    However, the clock is not output.
    We would like some advice.

  • Hi,

    very sorry for being so late in getting back to you. For some reason, I did not see it.

    You need to execute a sync command in order for the output clocks to be generated. You should enable the auto-sync mode in the Wizard for both DPLLs for the outputs to be generated right away.

    Then, the eval board cannot generate right away HCSL clocks. You need to set the jumpers P300, P301,..., P304 between pins 2 and 3 and then connect TP307 to TP308.

    Petre

Reply
  • Hi,

    very sorry for being so late in getting back to you. For some reason, I did not see it.

    You need to execute a sync command in order for the output clocks to be generated. You should enable the auto-sync mode in the Wizard for both DPLLs for the outputs to be generated right away.

    Then, the eval board cannot generate right away HCSL clocks. You need to set the jumpers P300, P301,..., P304 between pins 2 and 3 and then connect TP307 to TP308.

    Petre

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.