Post Go back to editing

AD9508 Input Clock Frequency Changes

Thread Summary

The user inquired about using the AD9508 as a frequency divider by 2, specifically whether it can handle rapid input frequency changes from 250 MHz to 1 GHz. The final answer confirms that the AD9508 can handle such variations, though the exact time for the transition is not specified. The engineer suggests that the transition might occur within a few nanoseconds in SPI mode.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD9508

Hi,

I want to use the AD9508 as a frequency divider by 2, without utilizing its phase adjustment functionality. My main concern is whether the chip can handle variations in the input signal frequency. For example, would it be an issue if the input frequency changes from 250 MHz to 1 GHz within a few microseconds ?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.