Post Go back to editing

Output Frequency Not Correct

Thread Summary

The user encountered incorrect output frequency in an LTC6990 VCO PLL simulation, suspecting a KCL issue. The problem was resolved by identifying a large input bias current (5 uA) of the LT6236 op-amp, which was not present in earlier simulations using ideal op-amp models. The final answer confirmed that the DIV resistor values should be scaled up to meet the 500 kOhm Thevenin equivalent resistance limit, and the user will avoid using the LT6236 in future designs.
AI Generated Content
Category: Hardware
Product Number: LTC6990

I'm using the LTC6990 as a VCO in a PLL.  I'd simulated with its model in the past with no issues, but now the output frequency is incorrect for a given control voltage.  The problem seems to be that the tool doesn't understand KCL.  Since the oscillator frequency is controlled by the current out of the "SET" pin (which is internally regulated to 1.0 V +/- 30 mV), I figured I'd just check the current there in the tool and compare that to what I'd expect it to be.  I got about 17 uA, which isn't anywhere near what it should have been.  What the current drawn from the SET pin should be can be easily calculated using KCL.  Please refer to the image below. (The loop has been broken and I have applied +2.5 VDC to the control input, expecting to get about 294 kHz out, but actually got about 420 kHz.)

VSET is about 1 V, as it should be.  The voltage at the op amp output, on the other side of R6 (374 kohms), is about 0.5 V, so the current flowing back through R6 should be (1.0 V - 0.5 V)/374k, which is about 1.34 uA.  The current flowing down through R7 should be (1 V)/96.2k, which is about 10.4 uA.  The current out of the SET pin should therefore be about 11.7 uA.  Measuring the current directly at the SET pin using the meter in the tool I get about 17 uA.  Is KCL no longer valid?  I cannot use this for any further simulations if the tool cannot calculate currents correctly.  I know the LTC6990 model only cares about what it thinks the current at the SET pin is, and that clearly is not correct.  Do you have any suggestions as to how i can deal with this?

Thank you.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.