I want to use LTC6906H in circuit that is rotating in the speed of 20000rpm.Is there is any problems to the output of ltc6906?.And also want the drawback of ltc6906H.
LTC6906
Production
The LTC6906 is a precision programmable oscillator that is versatile, compact and easy-to-use. Micropower operation benefits portable and battery-powered...
Datasheet
LTC6906 on Analog.com
I want to use LTC6906H in circuit that is rotating in the speed of 20000rpm.Is there is any problems to the output of ltc6906?.And also want the drawback of ltc6906H.
Hi George,
Can you provide a bit more detail to your question?
If I understand correctly, you want to use the LTC6906 in a high-G environment. What is the expected relative centrifugal g-force on the system?
Regarding output behavior and frequency accuracy, the LTC6906 oscillator is based on an RC circuit rather than a crystal. This makes it suitable for environments with high shock and vibration.
I couldn't understand what you mean by the drawback of LTC6906H.
Thanks,
Emrecan
My project is to convert voltage to frequency, so I am using the NA2100. To provide the clock frequency, I am using the LTC6906H. This circuit is placed inside a rotating fan operating at a speed of 20,000 RPM. Will there be any problems with the LTC6906H in the future?