Post Go back to editing

ADF4382A Agile LO Applications

Thread Summary

The user inquired about using the ADF4382A as an Agile LO, focusing on its fast calibration feature. The fast calibration time is 1us, but this does not necessarily mean the frequency can be switched in less than 1us. The engineer provided a GitHub repository link for the ADF4382 fast calibration feature implementation and a user guide for building and running the driver. The user also asked about using the ADF4382 with the pyiio-library and iio-oscilloscope on an SDP-S microcontroller, to which the engineer responded that the ADF4382 firmware is configured for SDP-K1 (STM32 microcontrollers) and suggested a build guide for custom firmware.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADF4382A

I am trying to understand if the ADF4382A can be used as a Agile LO for my application.

Reading the datasheet of the ADF4382A it appears to feature a "fast calibration of 1us".

Does that mean that I can switch the frequency of this part in less than 1us when using this feature?

If not, what is the tune time of this part? 

Thank you, Chris Corley