KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
ADCLK846
Recommended for New Designs
The ADCLK846 is a 1.2 GHz/250 MHz, LVDS/CMOS, fanout buffer optimized for low jitter and low power operation. Possible configurations range from 6 LVDS...
Datasheet
ADCLK846 on Analog.com
Hi,
Using a single-ended or a differential input to the ADCLK846 has not much effect on the propagation delay of the output. As seen on Figures 4 and 7, an input voltage level as small as 0.1Vpp and a common mode voltage as small as 200mV still has propagation delay of around 2ns.
Best regards,
Mark
Hi,
Using a single-ended or a differential input to the ADCLK846 has not much effect on the propagation delay of the output. As seen on Figures 4 and 7, an input voltage level as small as 0.1Vpp and a common mode voltage as small as 200mV still has propagation delay of around 2ns.
Best regards,
Mark