Hello,
i am working with the AD9546 in an Uni project. Having previously worked the the older AD9548 in our application, we are interested in trying to use the AD9546 due to the less complex circuit and atleast advertised better performance and size.
I have been trying to get the AD9546 to run properly for a week, with moderate success.
The setup is the following:
- 25MHz OCXO as system clock
- 1Hz PPS Input signal from a high quality GPS source
- 1Hz Output on OUT1BP, single ended.
My questions are:
- It seems to sync the output to the wrong edge of the reference (the falling Edge of the PPS) rather than the rising edge of the PPS (this is noticed by looking at the output compared to the input on an oscilloscope). Is this changeable?
- For some reason, the output does not be a square wave but to have a ~25% duty cycle
- It seems that the time for phase-lock takes long (>2 minutes). I have seen it multiple times on the forum that people dont use a setup like ours, but rather use the regular crystal on the devboard with an OCXO connected as a reference running in the AuxDPLL.
Is there any (performance/stability) benefit from using the OCXO as a compensating reference input rather than the system clock directly? Could this be a reason for the problems i am facing, which i should try out?
Looking forward to your responses, your help is very appreciated!
Best wishes
Matthias Nowak