Post Go back to editing

HMC7043 & HMC7044: Maximum frequency while using delay

Category: Datasheet/Specs
Product Number: HMC7043

Hello,

I have a question about the deference of "output channel" between HMC7043 and HMC7044.
The maximum output rate of HMC7043 using analog fine delay or digital coarse delay are different from HMC7044.
  The maximum analog fine delay frequency: 1600MHz(HMC7043, 3200MHz(HMC7044)
  The maximum digital coarse delay frequency: 1500MHz(HMC7043), 3200MHz(HMC7044)

I had understood the characteristics, the HMC7043 output channel and HMC7044 output channel, are the same. (Since both allow the same frequency input)
However, the specifications on the datasheet are not the same between HMC7043 and HMC7044 about this.
What is the reason for the difference?
Is the die different in the first place?

Best regards,

y_suzuki



modified the title
[edited by: y_suzuki at 2:33 AM (GMT -4) on 6 Sep 2024]