Post Go back to editing

AD9102: Testing the Output

Category: Hardware
Product Number: AD9102

Hi Experts,

I am using the AD9102 to create a square waveform.
The block diagram is below.



In the red square is the part that I would like to do the measurement.
This is my first time using a DAC to generate a square wave form, 
and wee need to test several features such as:

1) Signal Accuracy 
2) Noise
3) Overshoot/Undershoot
4) SNR (if it is possible for DAC)
5) Other parameters (ex THD if it is possible for DAC)

Questions:
1) From my Block Diagram in red, what kind of Test could I realize? 
2) What is the configuration of the test bench that I can provide for each test?


Thank you!
Filipe Satake