Post Go back to editing

How to generate a clock for synchronised with external 10 MHz sinus wave

Category: Hardware
Product Number: AD9548

Hello, 

I am working on a GNSS receiver that will process 12 bits I/Q data from an the AD9364. I would like to have the possibility to synchronise the receiver with an external sinus wave.

The idea is to use clock synchroniser to generate a CMOS clock to the AD9364 as the schema bellow.

Exemple of 10 MHz CW (50 ohm)

Do you think I should use AD9545 or AD9547 (AD9548) for the synchronisation ?

Or other components are more appriated?

These components seem to accept 10 MHz sinus wave. 

The external sinus wave is 10 MHz CW (50 ohm) between 5 to 11 dBm.

Thank you,

Patrice

Parents Reply Children
No Data