Hello,
I am working on a GNSS receiver that will process 12 bits I/Q data from an the AD9364. I would like to have the possibility to synchronise the receiver with an external sinus wave.
The idea is to use clock synchroniser to generate a CMOS clock to the AD9364 as the schema bellow.

Exemple of 10 MHz CW (50 ohm)

Do you think I should use AD9545 or AD9547 (AD9548) for the synchronisation ?
Or other components are more appriated?
These components seem to accept 10 MHz sinus wave.
The external sinus wave is 10 MHz CW (50 ohm) between 5 to 11 dBm.
Thank you,
Patrice