Post Go back to editing

PLL2 is not locking

Category: Hardware
Product Number: AD9523-1

Hello,

I am working on AD9523-1 customized board. in this new board, I'm having issue i.e. PLL2 is not getting locked. inputs that we are providing are REF A is 100 MHz, REF B is 10 MHz and VCXO input is 100 MHz. and the responses I'm getting are

at 0x22C - 0xE9, at 0x22D - 0x04, at 0x230 - 0x00, at 0x231 - 0x01, at 0x232 - 0x0D. and register map file giving to AD9523 is as follows:

"AD9523 Regmap File"
"Rev.","1.0"
""
"Addr(Hex)","Value(Bin)","Value(Hex)"
"0000","10000001","81"
"0002","00000000","00"
"0003","00000000","00"
"0004","00000000","00"
"0005","00000000","00"
"0006","00000000","00"
"0010","00000001","01"
"0011","00000000","00"
"0012","00000100","04"
"0013","00000000","00"
"0014","00000001","01"
"0015","00000000","00"
"0016","00101000","28"
"0017","00000000","00"
"0018","00001100","0C"
"0019","00011111","1F"
"001A","00010010","12"
"001B","00010110","16"
"001C","10010000","90"
"001D","00000000","00"
"001E","00000000","00"
"001F","00000000","00"
"0020","00000000","00"
"00F0","00000111","07"
"00F1","10000111","87"
"00F2","00010011","13"
"00F3","00000010","02"
"00F4","01000000","40"
"00F5","00000000","00"
"00F6","00000000","00"
"00F7","00000001","01"
"00F8","00000000","00"
"00F9","00000000","00"
"00FA","00000000","00"
"0190","01110011","73"
"0191","00001001","09"
"0192","00000100","04"
"0193","00100000","20"
"0194","00011111","1F"
"0195","00000100","04"
"0196","01001000","48"
"0197","01100011","63"
"0198","00000000","00"
"0199","01110110","76"
"019A","00011111","1F"
"019B","00000100","04"
"019C","01001000","48"
"019D","01100011","63"
"019E","00000000","00"
"019F","00100000","20"
"01A0","00011111","1F"
"01A1","00000100","04"
"01A2","00100000","20"
"01A3","00011111","1F"
"01A4","00000100","04"
"01A5","00100000","20"
"01A6","00011111","1F"
"01A7","00000100","04"
"01A8","01100110","66"
"01A9","00001001","09"
"01AA","00000100","04"
"01AB","01001001","49"
"01AC","01100011","63"
"01AD","00000000","00"
"01AE","01001001","49"
"01AF","01100011","63"
"01B0","00000000","00"
"01B1","01101000","68"
"01B2","00001001","09"
"01B3","00000100","04"
"01B4","01101000","68"
"01B5","00001001","09"
"01B6","00000100","04"
"01B7","01010110","56"
"01B8","00001001","09"
"01B9","00000000","00"
"01BA","00000000","00"
"01BB","00000000","00"
"022C","00000000","00"
"022D","00000000","00"
"022E","00000000","00"
"022F","00000000","00"
"0230","00000000","00"
"0231","00000001","01"
"0232","00001101","0D"
"0233","00000000","00"
"0234","00000001","01"
"0A00","00000000","00"
"0A01","00000000","00"
"0A02","00000000","00"
"0A03","00000010","02"
"0A04","00000000","00"
"0A05","00000100","04"
"0A06","00001110","0E"
"0A07","00000000","00"
"0A08","00010000","10"
"0A09","00001110","0E"
"0A0A","00000000","00"
"0A0B","11110000","F0"
"0A0C","00101011","2B"
"0A0D","00000001","01"
"0A0E","10010000","90"
"0A0F","00000001","01"
"0A10","00000001","01"
"0A11","11100000","E0"
"0A12","00000011","03"
"0A13","00000010","02"
"0A14","00110000","30"
"0A15","10000000","80"
"0A16","11111111","FF"
"0B00","00000000","00"
"0B01","00000000","00"
"0B02","00000000","00"
"0B03","00000000","00"

kindly help me in resolving this issue.

Parents Reply
  • Hello,

    Sorry to bother you but, as many of AD9523-1 ICs are performing in a same way i.e( PLL1 is locking but PLL2 is not locking) we thought "there was a problem in the lot where we had purchased" that's why we ordered brand new ICs. Among those new ICs we have tested 3 ICs and these 3 are also showing same performance(i.e. PLL1 is locking but PLL2 is not). so, Is there any possibility to make PLL2 also get locked.

Children