Post Go back to editing

PLL2 is not locking

Category: Hardware
Product Number: AD9523-1

Hello,

I am working on AD9523-1 customized board. in this new board, I'm having issue i.e. PLL2 is not getting locked. inputs that we are providing are REF A is 100 MHz, REF B is 10 MHz and VCXO input is 100 MHz. and the responses I'm getting are

at 0x22C - 0xE9, at 0x22D - 0x04, at 0x230 - 0x00, at 0x231 - 0x01, at 0x232 - 0x0D. and register map file giving to AD9523 is as follows:

"AD9523 Regmap File"
"Rev.","1.0"
""
"Addr(Hex)","Value(Bin)","Value(Hex)"
"0000","10000001","81"
"0002","00000000","00"
"0003","00000000","00"
"0004","00000000","00"
"0005","00000000","00"
"0006","00000000","00"
"0010","00000001","01"
"0011","00000000","00"
"0012","00000100","04"
"0013","00000000","00"
"0014","00000001","01"
"0015","00000000","00"
"0016","00101000","28"
"0017","00000000","00"
"0018","00001100","0C"
"0019","00011111","1F"
"001A","00010010","12"
"001B","00010110","16"
"001C","10010000","90"
"001D","00000000","00"
"001E","00000000","00"
"001F","00000000","00"
"0020","00000000","00"
"00F0","00000111","07"
"00F1","10000111","87"
"00F2","00010011","13"
"00F3","00000010","02"
"00F4","01000000","40"
"00F5","00000000","00"
"00F6","00000000","00"
"00F7","00000001","01"
"00F8","00000000","00"
"00F9","00000000","00"
"00FA","00000000","00"
"0190","01110011","73"
"0191","00001001","09"
"0192","00000100","04"
"0193","00100000","20"
"0194","00011111","1F"
"0195","00000100","04"
"0196","01001000","48"
"0197","01100011","63"
"0198","00000000","00"
"0199","01110110","76"
"019A","00011111","1F"
"019B","00000100","04"
"019C","01001000","48"
"019D","01100011","63"
"019E","00000000","00"
"019F","00100000","20"
"01A0","00011111","1F"
"01A1","00000100","04"
"01A2","00100000","20"
"01A3","00011111","1F"
"01A4","00000100","04"
"01A5","00100000","20"
"01A6","00011111","1F"
"01A7","00000100","04"
"01A8","01100110","66"
"01A9","00001001","09"
"01AA","00000100","04"
"01AB","01001001","49"
"01AC","01100011","63"
"01AD","00000000","00"
"01AE","01001001","49"
"01AF","01100011","63"
"01B0","00000000","00"
"01B1","01101000","68"
"01B2","00001001","09"
"01B3","00000100","04"
"01B4","01101000","68"
"01B5","00001001","09"
"01B6","00000100","04"
"01B7","01010110","56"
"01B8","00001001","09"
"01B9","00000000","00"
"01BA","00000000","00"
"01BB","00000000","00"
"022C","00000000","00"
"022D","00000000","00"
"022E","00000000","00"
"022F","00000000","00"
"0230","00000000","00"
"0231","00000001","01"
"0232","00001101","0D"
"0233","00000000","00"
"0234","00000001","01"
"0A00","00000000","00"
"0A01","00000000","00"
"0A02","00000000","00"
"0A03","00000010","02"
"0A04","00000000","00"
"0A05","00000100","04"
"0A06","00001110","0E"
"0A07","00000000","00"
"0A08","00010000","10"
"0A09","00001110","0E"
"0A0A","00000000","00"
"0A0B","11110000","F0"
"0A0C","00101011","2B"
"0A0D","00000001","01"
"0A0E","10010000","90"
"0A0F","00000001","01"
"0A10","00000001","01"
"0A11","11100000","E0"
"0A12","00000011","03"
"0A13","00000010","02"
"0A14","00110000","30"
"0A15","10000000","80"
"0A16","11111111","FF"
"0B00","00000000","00"
"0B01","00000000","00"
"0B02","00000000","00"
"0B03","00000000","00"

kindly help me in resolving this issue.

Parents
  • Hi,

    you say you want to configure the AD9523-1 to work with a VCXO=100MHz. Yet, the file you sent shows a VCXO=122.88MHz.

    Then the PLL2 was not configured correctly because it has a value lower than the min PLL2 VCO specification.

    Please tell me what output frequencies you need and I'll create a configuration for you. I already responded to you here:

     RE: How to set output frequency as 156.25 MHz ? 

    that the AD9523-1 cannot create 156.25MHz clocks.

    Petre

  • Hello,

    In one of the AD9523-1 board, if I select REF A input "0XEC" is the response from 0x22C register and from REF B  input "0xED" is the response from 0x22C register. I cant see the input signals accordingly  at REF A source and REF B source. I'm unable to find the problem that why these PLLs are not locking. 

  • here, I'm providing the configuration text file.

    "AD9523 Regmap File"
    "Rev.","1.0"
    ""
    "Addr(Hex)","Value(Bin)","Value(Hex)"
    "0000","10000001","81"
    "0002","00000000","00"
    "0003","00000000","00"
    "0004","00000000","00"
    "0005","00000000","00"
    "0006","00000000","00"
    "0010","00000100","04"
    "0011","00000000","00"
    "0012","00000100","04"
    "0013","00000000","00"
    "0014","00000001","01"
    "0015","00000000","00"
    "0016","00101000","28"
    "0017","00000000","00"
    "0018","00001100","0C"
    "0019","00011111","1F"
    "001A","00011010","1A"
    "001B","00010111","17"
    "001C","10010000","90"
    "001D","00000000","00"
    "001E","00000000","00"
    "001F","00000000","00"
    "0020","00000000","00"
    "00F0","00000111","07"
    "00F1","10000111","87"
    "00F2","00010011","13"
    "00F3","00000010","02"
    "00F4","01000000","40"
    "00F5","00000000","00"
    "00F6","00000000","00"
    "00F7","00000001","01"
    "00F8","00000000","00"
    "00F9","00000000","00"
    "00FA","00000000","00"
    "0190","01110011","73"
    "0191","00001001","09"
    "0192","00000100","04"
    "0193","00100000","20"
    "0194","00011111","1F"
    "0195","00000100","04"
    "0196","01001000","48"
    "0197","01100011","63"
    "0198","00000000","00"
    "0199","01110110","76"
    "019A","00011111","1F"
    "019B","00000100","04"
    "019C","01001000","48"
    "019D","01100011","63"
    "019E","00000000","00"
    "019F","00100000","20"
    "01A0","00011111","1F"
    "01A1","00000100","04"
    "01A2","00100000","20"
    "01A3","00011111","1F"
    "01A4","00000100","04"
    "01A5","00100000","20"
    "01A6","00011111","1F"
    "01A7","00000100","04"
    "01A8","01100110","66"
    "01A9","00001001","09"
    "01AA","00000100","04"
    "01AB","01001001","49"
    "01AC","01100011","63"
    "01AD","00000000","00"
    "01AE","01001001","49"
    "01AF","01100011","63"
    "01B0","00000000","00"
    "01B1","01101000","68"
    "01B2","00001001","09"
    "01B3","00000100","04"
    "01B4","01101000","68"
    "01B5","00001001","09"
    "01B6","00000100","04"
    "01B7","01010011","53"
    "01B8","00001001","09"
    "01B9","00000000","00"
    "01BA","00000000","00"
    "01BB","00000000","00"
    "022C","00000000","00"
    "022D","00000000","00"
    "022E","00000000","00"
    "022F","00000000","00"
    "0230","00000000","00"
    "0231","00000001","01"
    "0232","00001101","0D"
    "0233","00000000","00"
    "0234","00000001","01"
    "0A00","00000000","00"
    "0A01","00000000","00"
    "0A02","00000000","00"
    "0A03","00000010","02"
    "0A04","00000000","00"
    "0A05","00000100","04"
    "0A06","00001110","0E"
    "0A07","00000000","00"
    "0A08","00010000","10"
    "0A09","00001110","0E"
    "0A0A","00000000","00"
    "0A0B","11110000","F0"
    "0A0C","00101011","2B"
    "0A0D","00000001","01"
    "0A0E","10010000","90"
    "0A0F","00000001","01"
    "0A10","00000001","01"
    "0A11","11100000","E0"
    "0A12","00000011","03"
    "0A13","00000010","02"
    "0A14","00110000","30"
    "0A15","10000000","80"
    "0A16","11111111","FF"
    "0B00","00000000","00"
    "0B01","00000000","00"
    "0B02","00000000","00"
    "0B03","00000000","00"
    

  • Hi,

    I'm sorry, but you need to send me the stp file you created in order to extract the register values. I cannot upload this file to see what is going on.

    Petre

  • Hello,

    I'm also sorry,but while I'm trying to send stp file, I'm getting pop up like "unable to send the stp file". that's why I shared text file. you can convert it to stp file and upload. consider it kindly.

  • HI,

    When I converted your file to a file with a stp extension, and then I loaded it into the AD9523-1 evaluation software, I was given an error. I compared your file with a stp file I have, and they are different. I attach my file, which I used for our discussion. Compared it against yours. How did you obtain your file?

    ;Header contains information about the setup file and revision
    <Header>
         Product = AD9523-1
         FileVersion = 1.0
         DecimalSeparator=.    ;Used for internationalization
    </Header>
    
    <RegisterMap>
         &h0,&b00000001   ;01 Hex, 001 Dec
         &h2,&b00000000   ;00 Hex, 000 Dec
         &h3,&b00000000   ;00 Hex, 000 Dec
         &h4,&b00000000   ;00 Hex, 000 Dec
         &h5,&b00000000   ;00 Hex, 000 Dec
         &h6,&b00000000   ;00 Hex, 000 Dec
         &h10,&b00000001   ;01 Hex, 001 Dec
         &h11,&b00000000   ;00 Hex, 000 Dec
         &h12,&b00000100   ;04 Hex, 004 Dec
         &h13,&b00000000   ;00 Hex, 000 Dec
         &h14,&b00000001   ;01 Hex, 001 Dec
         &h15,&b00000000   ;00 Hex, 000 Dec
         &h16,&b00101000   ;28 Hex, 040 Dec
         &h17,&b00000000   ;00 Hex, 000 Dec
         &h18,&b00001100   ;0C Hex, 012 Dec
         &h19,&b00011111   ;1F Hex, 031 Dec
         &h1A,&b00010010   ;12 Hex, 018 Dec
         &h1B,&b00010110   ;16 Hex, 022 Dec
         &h1C,&b10010000   ;90 Hex, 144 Dec
         &h1D,&b00000000   ;00 Hex, 000 Dec
         &h1E,&b00000000   ;00 Hex, 000 Dec
         &h1F,&b00000000   ;00 Hex, 000 Dec
         &h20,&b00000000   ;00 Hex, 000 Dec
         &hF0,&b00000111   ;07 Hex, 007 Dec
         &hF1,&b10000111   ;87 Hex, 135 Dec
         &hF2,&b00010011   ;13 Hex, 019 Dec
         &hF3,&b00000010   ;02 Hex, 002 Dec
         &hF4,&b01000000   ;40 Hex, 064 Dec
         &hF5,&b00000000   ;00 Hex, 000 Dec
         &hF6,&b00000000   ;00 Hex, 000 Dec
         &hF7,&b00000001   ;01 Hex, 001 Dec
         &hF8,&b00000000   ;00 Hex, 000 Dec
         &hF9,&b00000000   ;00 Hex, 000 Dec
         &hFA,&b00000000   ;00 Hex, 000 Dec
         &h190,&b01110011   ;73 Hex, 115 Dec
         &h191,&b00001001   ;09 Hex, 009 Dec
         &h192,&b00000100   ;04 Hex, 004 Dec
         &h193,&b00100000   ;20 Hex, 032 Dec
         &h194,&b00011111   ;1F Hex, 031 Dec
         &h195,&b00000100   ;04 Hex, 004 Dec
         &h196,&b01001000   ;48 Hex, 072 Dec
         &h197,&b00001001   ;09 Hex, 009 Dec
         &h198,&b00000000   ;00 Hex, 000 Dec
         &h199,&b01110110   ;76 Hex, 118 Dec
         &h19A,&b00011111   ;1F Hex, 031 Dec
         &h19B,&b00000100   ;04 Hex, 004 Dec
         &h19C,&b01001000   ;48 Hex, 072 Dec
         &h19D,&b00001001   ;09 Hex, 009 Dec
         &h19E,&b00000000   ;00 Hex, 000 Dec
         &h19F,&b00100000   ;20 Hex, 032 Dec
         &h1A0,&b00011111   ;1F Hex, 031 Dec
         &h1A1,&b00000100   ;04 Hex, 004 Dec
         &h1A2,&b00100000   ;20 Hex, 032 Dec
         &h1A3,&b00011111   ;1F Hex, 031 Dec
         &h1A4,&b00000100   ;04 Hex, 004 Dec
         &h1A5,&b00100000   ;20 Hex, 032 Dec
         &h1A6,&b00011111   ;1F Hex, 031 Dec
         &h1A7,&b00000100   ;04 Hex, 004 Dec
         &h1A8,&b01100110   ;66 Hex, 102 Dec
         &h1A9,&b00001001   ;09 Hex, 009 Dec
         &h1AA,&b00000100   ;04 Hex, 004 Dec
         &h1AB,&b01001001   ;49 Hex, 073 Dec
         &h1AC,&b00001001   ;09 Hex, 009 Dec
         &h1AD,&b00000000   ;00 Hex, 000 Dec
         &h1AE,&b01001001   ;49 Hex, 073 Dec
         &h1AF,&b00001001   ;09 Hex, 009 Dec
         &h1B0,&b00000000   ;00 Hex, 000 Dec
         &h1B1,&b01101000   ;68 Hex, 104 Dec
         &h1B2,&b00001001   ;09 Hex, 009 Dec
         &h1B3,&b00000100   ;04 Hex, 004 Dec
         &h1B4,&b01101000   ;68 Hex, 104 Dec
         &h1B5,&b00001001   ;09 Hex, 009 Dec
         &h1B6,&b00000100   ;04 Hex, 004 Dec
         &h1B7,&b01010110   ;56 Hex, 086 Dec
         &h1B8,&b00001001   ;09 Hex, 009 Dec
         &h1B9,&b00000000   ;00 Hex, 000 Dec
         &h1BA,&b00000000   ;00 Hex, 000 Dec
         &h1BB,&b00000000   ;00 Hex, 000 Dec
         &h22C,&b00000000   ;00 Hex, 000 Dec
         &h22D,&b00000000   ;00 Hex, 000 Dec
         &h22E,&b00000000   ;00 Hex, 000 Dec
         &h22F,&b00000000   ;00 Hex, 000 Dec
         &h230,&b00000000   ;00 Hex, 000 Dec
         &h231,&b00000001   ;01 Hex, 001 Dec
         &h232,&b00000000   ;00 Hex, 000 Dec
         &h233,&b00000000   ;00 Hex, 000 Dec
         &h234,&b00000001   ;01 Hex, 001 Dec
         &hA00,&b00000000   ;00 Hex, 000 Dec
         &hA01,&b00000000   ;00 Hex, 000 Dec
         &hA02,&b00000000   ;00 Hex, 000 Dec
         &hA03,&b00000010   ;02 Hex, 002 Dec
         &hA04,&b00000000   ;00 Hex, 000 Dec
         &hA05,&b00000100   ;04 Hex, 004 Dec
         &hA06,&b00001110   ;0E Hex, 014 Dec
         &hA07,&b00000000   ;00 Hex, 000 Dec
         &hA08,&b00010000   ;10 Hex, 016 Dec
         &hA09,&b00001110   ;0E Hex, 014 Dec
         &hA0A,&b00000000   ;00 Hex, 000 Dec
         &hA0B,&b11110000   ;F0 Hex, 240 Dec
         &hA0C,&b00101011   ;2B Hex, 043 Dec
         &hA0D,&b00000001   ;01 Hex, 001 Dec
         &hA0E,&b10010000   ;90 Hex, 144 Dec
         &hA0F,&b00000001   ;01 Hex, 001 Dec
         &hA10,&b00000001   ;01 Hex, 001 Dec
         &hA11,&b11100000   ;E0 Hex, 224 Dec
         &hA12,&b00000011   ;03 Hex, 003 Dec
         &hA13,&b00000010   ;02 Hex, 002 Dec
         &hA14,&b00110000   ;30 Hex, 048 Dec
         &hA15,&b10000000   ;80 Hex, 128 Dec
         &hA16,&b11111111   ;FF Hex, 255 Dec
         &hB00,&b00000000   ;00 Hex, 000 Dec
         &hB01,&b00000000   ;00 Hex, 000 Dec
         &hB02,&b00000000   ;00 Hex, 000 Dec
         &hB03,&b00000000   ;00 Hex, 000 Dec
    </RegisterMap>
    
    <PinStates>
         PortA=&h1E ;Bit0=USBStatus, Bit1=CSB, Bit2=ResetB, Bit3=SyncB, Bit4=PDB, Bit5=RefSel
    </PinStates>
    
    <SoftwareSettings>
         AutoSendUpdate=1              ;AutoIOUpdate Setting
         REF_A = 10.0000
         REF_B = 10.0000
         REF_TEST = 10.0000
         VCXO = 100.0000
    </SoftwareSettings>
    

    Petre

  • Hello Petre,

    I obtained my text file from AD9523-1 Evaluation software. I'm trying in this way i.e view->debug window->load register map for loading the text file, view->debug window->save register map for getting the configuration that I set in the software in text format. and I compared your stp file with my text file and yes, both are different. now, we are also using REF A 100 MHz input and the schematic is as follows. based on the schematic would you please tell me what configuration can I set to REF A input(i.e single ended or differential etc,.)

    and to this board PLL2 is not locking with REF B input,what modifications can I do for PLL2 gets locked.

  • Hi,

    Thanks for the tip. I was able to load the register values you sent. Next time, please save the configuration from File, Save Setup function. and send it to me.

    These are my comments about the configuration and schematic (which is not very clear. If you could send a more accurate, photo, it would be better):

    - the PLL2 charge pump current is too small at 24.5 uA. I recommend to bring that current up to at least 882.0 uA. Disable the anti-backlash period.

    - If REFA=100 MHz, then set the REFA=40.

    - VCXO is set for the negative SE input, but the schematic shows the OSC_IN pin ac coupled to a VCXO pin. You need to take that pin and ac couple it to ground. Measure the clock at OSC_IN\ pin to verify it is a 3.3V CMOS clock.

    Let's see if you can get the PLL2 to lock. I cannot verify the configuration because I do not have a board with VCXO=100MHz. I have one with VCXO=122.88MHz, and your configuration makes the PLL2 VCO to be out of range.

    Petre

  • Hello,

    I tried in 2 different ways. 

    the PLL2 charge pump current is too small at 24.5 uA. I recommend to bring that current up to at least 882.0 uA. Disable the anti-backlash period.

    I tried with these software changes, without grounding the OSC_IN pin, then both the PLLs got locked once and again came back to only PLL1 locking state.

    later I grounded OSC_IN PIN, then PLL2 is not locking even for once.

    Here is the schematic PDF like this, but R15,R17,C19,R26 and C26 components were not mounted.

    And configuration I kept(i.e. Ref_A_Ref_Bconfiguration.txt) is working with one board but not with the other board. so, I'm doubting on the hardware but I can't find the issue.  

  • HI,

    you cannot leave the pin 9, OSC_IN floating. Please send me the Y2 data sheet to take a look. How is it possible that on the other board, PLL2 locks and on this one does not? 

    Petre

Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.