Post Go back to editing

How to set output frequency as 156.25 MHz ?

Category: Software
Product Number: AD9523-1
Software Version: AD9523 - 1 evaluation software

I'm working on AD9523-1 evaluation software, providing REF A as 100MHz , REF B as 10 MHz and external VCXO as 100MHz. I'm trying to set the output frequency as 156.25 MHz but unable to do that.please suggest me the settings to set the output frequency as 156.25 MHz.

Parents
  • Hi,

    I'm sorry to tell you, but it does not seem you'll be able to generate 156.25MHz with the AD9523-1. You can set the PLL2 VCO to 156.25E6*19=2968.75MHz, which makes the total dividing factor of the output be 19. The PLL2 VCO may be divided first by a number equal to 3, 4, or 5, which are not factors of 19.

    So independent of the VCXO value you choose, the AD9523-1 cannot be configured to create 156.25MHz.

    Take a look at the AD9528, which is very similar as architecture with the AD9523-1 and with a VCXO=100MHz, you could generate 156.25MHz clocks.

    See attached the stp file I created for the AD9528. I did not test it on a board, but it should function.

    Petre

    <header>
    product = AD9528
    softwareversion = 1.0.0.3
    </header>
    
    <detailed setup information>
    -- PLL1 --
     - Ref A -
        Input Freq: 100.0 MHz
        Ra: 10
        PFD Freq: 10.0 MHz
     - Ref B -
        Input Freq: 10.0 MHz
        Rb: 1
        PFD Freq: 10.0 MHz
     - Clk In -
        Osc Freq: 100.0 MHz
        N1: 10
        PFD Freq: 10.0 MHz
    ------------------
    -- PLL2 --
        Input Freq: 50.0 MHz
        R2: /2
        PFD Freq: 100.0 MHz
        N2: 25
        Dist Freq: 1.25 GHz
        M: 3
        VCO Freq: 3.75 GHz
    ----------------------
    -- SysRef --
        Source: External SysRef
        Freq: 768.0 kHz
    ----------------------
    -- Distribution --
        Input Source: PLL2
        Input Freq: 1.25 GHz
     - Out 0 -
        Input Source: D0
        D0:8
        Output Freq: 156.25 MHz
     - Out 1 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 2 -
        Input Source: D2
        D2:5
        Output Freq: 250.0 MHz
     - Out 3 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 4 -
        Input Source: D4
        D4:5
        Output Freq: 250.0 MHz
     - Out 5 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 6 -
        Input Source: D6
        D6:5
        Output Freq: 250.0 MHz
     - Out 7 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 8 -
        Input Source: D8
        D8:5
        Output Freq: 250.0 MHz
     - Out 9 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 10 -
        Input Source: D10
        D10:5
        Output Freq: 250.0 MHz
     - Out 11 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 12 -
        Input Source: PLL1
        Output Freq: 100.0 MHz
     - Out 13 -
        Input Source: PLL1
        Output Freq: 100.0 MHz
    ----------------------
    </detailed setup information>
    
    <registers>
    Register (Hex),	Value (Hex),	Value (Dec)
    0x0,		0x00,		0
    0x1,		0x00,		0
    0x3,		0x05,		5
    0x4,		0xFF,		255
    0x5,		0x00,		0
    0x6,		0x03,		3
    0xa,		0x00,		0
    0xb,		0x00,		0
    0xc,		0x56,		86
    0xd,		0x04,		4
    0xf,		0x00,		0
    0x100,		0x0A,		10
    0x101,		0x00,		0
    0x102,		0x01,		1
    0x103,		0x00,		0
    0x104,		0x0A,		10
    0x105,		0x00,		0
    0x106,		0x0C,		12
    0x107,		0x03,		3
    0x108,		0x18,		24
    0x109,		0x04,		4
    0x10a,		0x00,		0
    0x10b,		0x00,		0
    0x200,		0xFF,		255
    0x201,		0xD2,		210
    0x202,		0x03,		3
    0x203,		0x10,		16
    0x204,		0x03,		3
    0x205,		0x00,		0
    0x206,		0x00,		0
    0x207,		0x02,		2
    0x208,		0x18,		24
    0x209,		0x00,		0
    0x300,		0x00,		0
    0x301,		0x00,		0
    0x302,		0x07,		7
    0x303,		0x40,		64
    0x304,		0x00,		0
    0x305,		0x00,		0
    0x306,		0x00,		0
    0x307,		0x00,		0
    0x308,		0x04,		4
    0x309,		0x40,		64
    0x30a,		0x00,		0
    0x30b,		0x00,		0
    0x30c,		0x00,		0
    0x30d,		0x00,		0
    0x30e,		0x04,		4
    0x30f,		0x40,		64
    0x310,		0x00,		0
    0x311,		0x00,		0
    0x312,		0x00,		0
    0x313,		0x00,		0
    0x314,		0x04,		4
    0x315,		0x40,		64
    0x316,		0x00,		0
    0x317,		0x00,		0
    0x318,		0x00,		0
    0x319,		0x00,		0
    0x31a,		0x04,		4
    0x31b,		0x40,		64
    0x31c,		0x00,		0
    0x31d,		0x00,		0
    0x31e,		0x00,		0
    0x31f,		0x00,		0
    0x320,		0x04,		4
    0x321,		0x40,		64
    0x322,		0x00,		0
    0x323,		0x00,		0
    0x324,		0x20,		32
    0x325,		0x00,		0
    0x326,		0x00,		0
    0x327,		0x20,		32
    0x328,		0x00,		0
    0x329,		0x00,		0
    0x32a,		0x00,		0
    0x32b,		0x00,		0
    0x32c,		0x00,		0
    0x32d,		0x00,		0
    0x32e,		0x00,		0
    0x400,		0x00,		0
    0x401,		0x00,		0
    0x402,		0x00,		0
    0x403,		0x00,		0
    0x404,		0x04,		4
    0x500,		0x10,		16
    0x501,		0x00,		0
    0x502,		0x00,		0
    0x503,		0xFF,		255
    0x504,		0xFF,		255
    0x505,		0x00,		0
    0x506,		0x00,		0
    0x507,		0x00,		0
    0x508,		0x00,		0
    0x509,		0x00,		0
    </registers>
    
    <frequencies>
    100000000;10000000;100000000;768000
    </frequencies>
    
     

Reply
  • Hi,

    I'm sorry to tell you, but it does not seem you'll be able to generate 156.25MHz with the AD9523-1. You can set the PLL2 VCO to 156.25E6*19=2968.75MHz, which makes the total dividing factor of the output be 19. The PLL2 VCO may be divided first by a number equal to 3, 4, or 5, which are not factors of 19.

    So independent of the VCXO value you choose, the AD9523-1 cannot be configured to create 156.25MHz.

    Take a look at the AD9528, which is very similar as architecture with the AD9523-1 and with a VCXO=100MHz, you could generate 156.25MHz clocks.

    See attached the stp file I created for the AD9528. I did not test it on a board, but it should function.

    Petre

    <header>
    product = AD9528
    softwareversion = 1.0.0.3
    </header>
    
    <detailed setup information>
    -- PLL1 --
     - Ref A -
        Input Freq: 100.0 MHz
        Ra: 10
        PFD Freq: 10.0 MHz
     - Ref B -
        Input Freq: 10.0 MHz
        Rb: 1
        PFD Freq: 10.0 MHz
     - Clk In -
        Osc Freq: 100.0 MHz
        N1: 10
        PFD Freq: 10.0 MHz
    ------------------
    -- PLL2 --
        Input Freq: 50.0 MHz
        R2: /2
        PFD Freq: 100.0 MHz
        N2: 25
        Dist Freq: 1.25 GHz
        M: 3
        VCO Freq: 3.75 GHz
    ----------------------
    -- SysRef --
        Source: External SysRef
        Freq: 768.0 kHz
    ----------------------
    -- Distribution --
        Input Source: PLL2
        Input Freq: 1.25 GHz
     - Out 0 -
        Input Source: D0
        D0:8
        Output Freq: 156.25 MHz
     - Out 1 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 2 -
        Input Source: D2
        D2:5
        Output Freq: 250.0 MHz
     - Out 3 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 4 -
        Input Source: D4
        D4:5
        Output Freq: 250.0 MHz
     - Out 5 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 6 -
        Input Source: D6
        D6:5
        Output Freq: 250.0 MHz
     - Out 7 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 8 -
        Input Source: D8
        D8:5
        Output Freq: 250.0 MHz
     - Out 9 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 10 -
        Input Source: D10
        D10:5
        Output Freq: 250.0 MHz
     - Out 11 -
        Input Source: Sysref
        Output Freq: 768.0 kHz
     - Out 12 -
        Input Source: PLL1
        Output Freq: 100.0 MHz
     - Out 13 -
        Input Source: PLL1
        Output Freq: 100.0 MHz
    ----------------------
    </detailed setup information>
    
    <registers>
    Register (Hex),	Value (Hex),	Value (Dec)
    0x0,		0x00,		0
    0x1,		0x00,		0
    0x3,		0x05,		5
    0x4,		0xFF,		255
    0x5,		0x00,		0
    0x6,		0x03,		3
    0xa,		0x00,		0
    0xb,		0x00,		0
    0xc,		0x56,		86
    0xd,		0x04,		4
    0xf,		0x00,		0
    0x100,		0x0A,		10
    0x101,		0x00,		0
    0x102,		0x01,		1
    0x103,		0x00,		0
    0x104,		0x0A,		10
    0x105,		0x00,		0
    0x106,		0x0C,		12
    0x107,		0x03,		3
    0x108,		0x18,		24
    0x109,		0x04,		4
    0x10a,		0x00,		0
    0x10b,		0x00,		0
    0x200,		0xFF,		255
    0x201,		0xD2,		210
    0x202,		0x03,		3
    0x203,		0x10,		16
    0x204,		0x03,		3
    0x205,		0x00,		0
    0x206,		0x00,		0
    0x207,		0x02,		2
    0x208,		0x18,		24
    0x209,		0x00,		0
    0x300,		0x00,		0
    0x301,		0x00,		0
    0x302,		0x07,		7
    0x303,		0x40,		64
    0x304,		0x00,		0
    0x305,		0x00,		0
    0x306,		0x00,		0
    0x307,		0x00,		0
    0x308,		0x04,		4
    0x309,		0x40,		64
    0x30a,		0x00,		0
    0x30b,		0x00,		0
    0x30c,		0x00,		0
    0x30d,		0x00,		0
    0x30e,		0x04,		4
    0x30f,		0x40,		64
    0x310,		0x00,		0
    0x311,		0x00,		0
    0x312,		0x00,		0
    0x313,		0x00,		0
    0x314,		0x04,		4
    0x315,		0x40,		64
    0x316,		0x00,		0
    0x317,		0x00,		0
    0x318,		0x00,		0
    0x319,		0x00,		0
    0x31a,		0x04,		4
    0x31b,		0x40,		64
    0x31c,		0x00,		0
    0x31d,		0x00,		0
    0x31e,		0x00,		0
    0x31f,		0x00,		0
    0x320,		0x04,		4
    0x321,		0x40,		64
    0x322,		0x00,		0
    0x323,		0x00,		0
    0x324,		0x20,		32
    0x325,		0x00,		0
    0x326,		0x00,		0
    0x327,		0x20,		32
    0x328,		0x00,		0
    0x329,		0x00,		0
    0x32a,		0x00,		0
    0x32b,		0x00,		0
    0x32c,		0x00,		0
    0x32d,		0x00,		0
    0x32e,		0x00,		0
    0x400,		0x00,		0
    0x401,		0x00,		0
    0x402,		0x00,		0
    0x403,		0x00,		0
    0x404,		0x04,		4
    0x500,		0x10,		16
    0x501,		0x00,		0
    0x502,		0x00,		0
    0x503,		0xFF,		255
    0x504,		0xFF,		255
    0x505,		0x00,		0
    0x506,		0x00,		0
    0x507,		0x00,		0
    0x508,		0x00,		0
    0x509,		0x00,		0
    </registers>
    
    <frequencies>
    100000000;10000000;100000000;768000
    </frequencies>
    
     

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.