Post Go back to editing

Input Frequency Range for ADCLK925.

Thread Summary

The user is looking for a replacement for the LTC6957, considering the ADCLK925. The ADCLK925 supports an input frequency range from 10 Hz to 6 GHz, suitable for the user's previous 10 MHz clock application.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADCLK925

Hello, 

I received the LTC6957 discontinuation notice. So I am considering the ADCLK925 as a replacement for that part. But I can't find the Input frequency range in the datasheet of that part. Could you tell me the minimum and maximum input frequency range?

I had previously applied 10MHz clock into LTC6957.

Thanks.