Post Go back to editing

LTC6954 CMOS output 50ohm drive capability

Category: Hardware
Product Number: LTC6954

Hello,

I would like to clock a component on a different board than the one where my LTC6954-3 is sitting.

I see that in the "Common output interface configuration" you don't display a far termination, therefore I concluded that the device is not capable of driving a 50ohm load. Am I correct ?

If that's the case, is there driver you would recommend to drive a square 40MHz 1.8V CMOS input device with SMA connection ?

Thanks a lot for you valuable help,

Regards,

Gaël

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.