Hi,
I have a query w.r.t HMC7043 clock distributor.
Pg 20 of datasheet (www.analog.com/.../HMC7043.pdf) states the following to avoid creating a runt pulse:
"The situation is avoided by never applying phase offset more
than (50% − 8) clock input cycles to an output channel
configured as a pulse generator."
Can someone help me understand what does (50% - 8) clock input cycle mean? Also how we can calculate the above value (here is 8 being subtracted from 50 % ?) . How can we verify that phase offset < (50% -8) clock input cycles.
Thanks,
Merlyn