Hi Sir,
I found that in the material content declaration of this part number, it shows complies with JS709 low halogen definition, that means the maximum concentration of Br is 1000 ppm from BFRs, the maximum concentration of Cl is 1000 ppm from CFRs or PVC etc.
But in the information on enviromental compliance site, ADI defines halogen free within a homogeneous material to mean the maximum concentration of Br is 900 ppm, the maximum concentration of Cl is 900 ppm, and the maximum concentration of total Br + Cl is 1500 ppm.
Can you clarify or provide a declaration? I'm not sure if this material is halogen-free in the standard sense.
thank you.