Post Go back to editing

AD9576 no output on my board

Thread Summary

The user is experiencing no output and I2C communication issues with the AD9576 on a custom PCB. The final answer suggests using an AD9576 evaluation board to verify functionality, removing the RC delay from the /RESET pin, and ensuring the RESETB pulse is at least 1.25ns. The user should also check if the custom PCB schematic matches the eval board schematic.
AI Generated Content
Category: Hardware
Product Number: AD9576

Hi ADI experts,

Now I'm using AD9576 on my self-designed PCB. I set PPR0=0, PPR2=0, PPR3=2. Use a XTAL for REF0. FER1 and REF2 are all floating.

Use an external RC delay for /RESET pin. 

A single 3.3V for all power pins.

After power on, there is no output on any output pins. The XTAL doesn't have any signal measured by oscilloscope.

We also try to communicate with AD9576 by I2C(There are pull up resistors to 3.3V at master side), but no ACK is received from AD9576. Also, after I2C communication try fail, the I2C bus will be hold at about 1.7V level.

I don't know why. Thank.

Parents Reply Children
No Data