Post Go back to editing

Clock chip 9528 spi probe fails with error -14

Category: Software

Hi,

We have a custom board with zu11eg running petalinux and xcvr AD9026, where AD9528 Clock chip is tied to spi CSS2. The clock chip is added as a jesd device.

During boot The spi initialization fails with error code -14. If you remove the jesd device declaration, then we don't see the error, but the rest of the jesd topology cannot find ad9528 and therefore do not get initialized. Is there anyone who experienced the same, or point me to the right direction please. Thanks

root@zynqmp-iwg35m:~# dmesg | grep 9528
[ 2.232977] jesd204: created con: id=3, topo=10, link=3, /axi/spi@ff040000/ad9528-1@0 <-> /fpga-axi@0/axi_adxcvr@a0080000
[ 2.233006] jesd204: created con: id=4, topo=10, link=0, /axi/spi@ff040000/ad9528-1@0 <-> /fpga-axi@0/axi_adxcvr@a0040000
[ 2.233037] jesd204: created con: id=5, topo=10, link=2, /axi/spi@ff040000/ad9528-1@0 <-> /fpga-axi@0/axi_adxcvr@a0000000
[ 5.230237] ad9528 spi0.2: supply vcc not found, using dummy regulator
[ 5.267192] jesd204: /axi/spi@ff040000/ad9528-1@0,jesd204:1,parent=spi0.2: Device isn't a top-device, nor does it belong to topology with top-device
[ 5.280512] ad9528: probe of spi0.2 failed with error -14

device tree entry:

&spi0 {
	status = "okay";
	num-cs = <3>;
	is-decoded-cs = <0>;

	#address-cells = <1>;
	#size-cells = <0>;

	clk0_ad9528: ad9528-1@0 {
		compatible = "adi,ad9528";

		jesd204-device;
		#jesd204-cells = <2>;
		jesd204-sysref-provider;

		reg = <2>;
		#address-cells = <1>;
		#size-cells = <0>;

		spi-max-frequency = <10000000>;		
		spi-cpol;
		spi-cpha;

		clock-output-names = "ad9528-1_out0", "ad9528-1_out1", "ad9528-1_out2",
			"ad9528-1_out3", "ad9528-1_out4", "ad9528-1_out5", "ad9528-1_out6",
			"ad9528-1_out7", "ad9528-1_out8", "ad9528-1_out9", "ad9528-1_out10",
			"ad9528-1_out11", "ad9528-1_out12", "ad9528-1_out13";
		#clock-cells = <1>;

		adi,vcxo-freq = <100000000>;
		/* adi,osc-diff-rcv-enable; */

		/* PLL1 config - not needed */
		/* disable both reference inputs
		adi,refa-enable;
		adi,refa-diff-rcv-e;
		adi,refa-r-div = <1>;
		adi,osc-in-cmos-neg-inp-enable;
		adi,pll1-feedback-div = <10>;
		adi,pll1-charge-pump-current-nA = <6000>; */

		/* PLL2 config */
		adi,pll2-m1-frequency = <1000000000>;
		
		/* This is redundant
		adi,pll2-vco-div-m1 = <4>;
		adi,pll2-n2-div = <10>; */ /* N / M1 */

		adi,pll2-r1-div = <1>;
		adi,pll2-charge-pump-current-nA = <806000>;

		/* SYSREF config */
		adi,sysref-src = <SYSREF_SRC_INTERNAL>;
		adi,sysref-pattern-mode = <SYSREF_PATTERN_CONTINUOUS>;
		adi,sysref-k-div = <512>;
		adi,sysref-request-enable;
		adi,sysref-nshot-mode = <SYSREF_NSHOT_4_PULSES>;
		adi,sysref-request-trigger-mode = <SYSREF_LEVEL_HIGH>;

		adi,rpole2 = <RPOLE2_900_OHM>;
		adi,rzero = <RZERO_1850_OHM>;
		adi,cpole1 = <CPOLE1_16_PF>;

		adi,status-mon-pin0-function-select = <1>; /* PLL1 & PLL2 Locked */
		adi,status-mon-pin1-function-select = <7>; /* REFA Correct */

		ad9528_0_c0: channel@0 {
			reg = <0>;
			adi,extended-name = "DEV_CLK_TEST";
			adi,driver-mode = <DRIVER_MODE_LVDS>;
			adi,divider-phase = <0>;
			adi,channel-divider = <4>;
			adi,signal-source = <SOURCE_VCO>;
		};
		
		ad9528_0_c5: channel@5 {
			reg = <5>;
			adi,extended-name = "DEV_CLK";
			adi,driver-mode = <DRIVER_MODE_LVDS>;
			adi,divider-phase = <4>;
			adi,channel-divider = <4>;
			adi,signal-source = <SOURCE_VCO>;
		};

		ad9528_0_c7: channel@7 {
			reg = <7>;
			adi,extended-name = "DEV_SYSREF";
			adi,driver-mode = <DRIVER_MODE_LVDS>;
			adi,divider-phase = <8>;
			adi,channel-divider = <8>;
			adi,signal-source = <SOURCE_VCO>;
		};

		ad9528_0_c9: channel@9 {
			reg = <9>;
			adi,extended-name = "FPGA_SYSREF";
			adi,driver-mode = <DRIVER_MODE_LVDS>;
			adi,divider-phase = <8>;
			adi,channel-divider = <8>;
			adi,signal-source = <SOURCE_SYSREF_VCO>;
		};

		ad9528_0_c10: channel@10 {
			reg = <10>;
			adi,extended-name = "FPGA_REFCLK";
			adi,driver-mode = <DRIVER_MODE_LVDS>;
			adi,divider-phase = <4>;
			adi,channel-divider = <4>;
			adi,signal-source = <SOURCE_SYSREF_VCO>;
		};
	};

};

Parents Reply Children
  • Thanks. The issue I reported elsewhere is not the same, and I don't think its related to the board or platform I am using. When I declare 9528 as a jesd device it fails to initialize, but if I remove the jesd fsm framework declarations from the device tree it comes up. If this community cannot support the platform, I understand. Appreciate your time.

  • For anyone who is having the same issue, I fixed it by moving the jesd declarations to a separate dtsi file and including it at the bottom of my custom dts. The final device tree entree looks like this:

    === in my custom dts file ==

    clk0_ad9528: ad9528-1@0 {


    compatible = "adi,ad9528";

    reg = <2>;
    #address-cells = <1>;
    #size-cells = <0>;

    spi-max-frequency = <10000000>;
    /*spi-cpol;
    spi-cpha;*/
    reset-gpios = <&axi_gpio 1 GPIO_ACTIVE_LOW>;

    clock-output-names = "ad9528-1_out0", "ad9528-1_out1", "ad9528-1_out2",
    "ad9528-1_out3", "ad9528-1_out4", "ad9528-1_out5", "ad9528-1_out6",
    "ad9528-1_out7", "ad9528-1_out8", "ad9528-1_out9", "ad9528-1_out10",
    "ad9528-1_out11", "ad9528-1_out12", "ad9528-1_out13";
    #clock-cells = <1>;

    adi,vcxo-freq = <100000000>;

    /* PLL2 config */
    adi,pll2-m1-frequency = <1000000000>;
    adi,pll2-r1-div = <1>;
    adi,pll2-charge-pump-current-nA = <806000>;

    /* SYSREF config */
    adi,sysref-src = <SYSREF_SRC_INTERNAL>;
    adi,sysref-pattern-mode = <SYSREF_PATTERN_CONTINUOUS>;
    adi,sysref-k-div = <500>;
    adi,sysref-nshot-mode = <SYSREF_NSHOT_4_PULSES>;
    adi,sysref-request-trigger-mode = <SYSREF_LEVEL_HIGH>;

    adi,rpole2 = <RPOLE2_900_OHM>;
    adi,rzero = <RZERO_1850_OHM>;
    adi,cpole1 = <CPOLE1_16_PF>;

    adi,status-mon-pin0-function-select = <1>; /* PLL1 & PLL2 Locked */
    adi,status-mon-pin1-function-select = <7>; /* REFA Correct */

    ad9528_0_c0: channel@0 {
    reg = <0>;
    adi,extended-name = "DEV_CLK_TEST";
    adi,driver-mode = <DRIVER_MODE_LVDS>;
    adi,divider-phase = <0>;
    adi,channel-divider = <4>;
    adi,signal-source = <SOURCE_VCO>;
    };

    ad9528_0_c5: channel@5 {
    reg = <5>;
    adi,extended-name = "FPGA_REFCLK";
    adi,driver-mode = <DRIVER_MODE_LVDS>;
    adi,divider-phase = <4>;
    adi,channel-divider = <4>;
    adi,signal-source = <SOURCE_VCO>;
    };

    ad9528_0_c9: channel@9 {
    reg = <9>;
    adi,extended-name = "DEV_SYSREF";
    adi,driver-mode = <DRIVER_MODE_LVDS>;
    adi,divider-phase = <0>;
    adi,channel-divider = <256>;
    adi,signal-source = <SOURCE_SYSREF_VCO>;
    };

    ad9528_0_c10: channel@10 {
    reg = <10>;
    adi,extended-name = "DEV_CLK";
    adi,driver-mode = <DRIVER_MODE_LVDS>;
    adi,divider-phase = <4>;
    adi,channel-divider = <4>;
    adi,signal-source = <SOURCE_VCO>;
    };

    ad9528_0_c11: channel@11 {
    reg = <11>;
    adi,extended-name = "FPGA_SYSREF";
    adi,driver-mode = <DRIVER_MODE_LVDS>;
    adi,divider-phase = <0>;
    adi,channel-divider = <256>;
    adi,signal-source = <SOURCE_SYSREF_VCO>;
    };

    };

    ==== In a separate dts file (which is included at the bottom of my custom dts ====

    &clk0_ad9528 {
        jesd204-device;
        #jesd204-cells = <2>;
        jesd204-sysref-provider;
    };