Post Go back to editing

No lock

Category: Hardware
Product Number: LTC6951

Hi,

We have a design with the LTC6951 on a custom board with a reference clock of 25 MHz.

The target is a VCO frequency of 4800 MHz but the PLL is only able to lock in the frequency range of 4175 to 4350 MHz.

When it is set to 4800, it is not locked and the output frequencies are corresponding to 4350 MHz on the VCO and VTUNE is around 4V.

It seems like the calibration is not working, but it is manually triggered and AUTOCAL is enabled so it should trigger after registers 0x05 and 0x06. Also BD is 96 according to Fpfd = 25 MHz.

The reference clock flag is marked as OK. Below are the schematics and configuration of the PLL.

I am aware that the loop filter is not the optimum for the thermal noise in this configuration, I have modified it to get it close to the calculated in the software tool (for 1mA) and still the same behavior.

So what can be the reason is not locking outside of that frequency range?

Thanks in advance,

Marta

        ltc6951_spi_write(0, LTC6951_REG_01, 0x3A);    // STAT output config
        ltc6951_spi_write(0, LTC6951_REG_02, 0x00);    // Power downs and CAL trigger
        ltc6951_spi_write(0, LTC6951_REG_03, 0x78);    // AUTOCAL 1, RAO     0, BST 0, FLT 0
        ltc6951_spi_write(0, LTC6951_REG_04, 0x70);    // B    96
        ltc6951_spi_write(0, LTC6951_REG_05, 0x04);    // R    1
        ltc6951_spi_write(0, LTC6951_REG_06, 0xC0);    // N    192
        ltc6951_spi_write(0, LTC6951_REG_07, 0x00);    // CP 1mA
        ltc6951_spi_write(0, LTC6951_REG_08, 0x00);    // P    2
        ltc6951_spi_write(0, LTC6951_REG_09, 0x30); //OUT0    OFF
        ltc6951_spi_write(0, LTC6951_REG_0A, 0x03);
        ltc6951_spi_write(0, LTC6951_REG_0B, 0x11); //OUT1    1200 MHz    M1    2
        ltc6951_spi_write(0, LTC6951_REG_0C, 0x00);
        ltc6951_spi_write(0, LTC6951_REG_0D, 0x03); //OUT2    OFF
        ltc6951_spi_write(0, LTC6951_REG_0E, 0x00);
        ltc6951_spi_write(0, LTC6951_REG_0F, 0x16); //OUT3    100 MHz        M3    24
        ltc6951_spi_write(0, LTC6951_REG_10, 0x00);
        ltc6951_spi_write(0, LTC6951_REG_11, 0x18); //OUT4    50 MHz        M4    48
        ltc6951_spi_write(0, LTC6951_REG_12, 0x00);


        ltc6951_spi_write(0, LTC6951_REG_02, 0x01);    // Trigger manual calibration

  • Hi  

    When I checked your register settings, I saw that REG0x03 is set to 0x78. However, you screenshot shows that none of the ALCCAL, ALCEN or ALCULOK is enabled. The ALC must be allowed to operate during or after a calibration cycle. At least one of the ALCCAL, ALCEN, or ALCULOK bits must be set.

    Can you check that there is no problem at writing to the LTC6951?

    Thanks,

    Emrecan

  • Hi Emrecan,

    Thanks for your reaction!

    I am using it as in the registers so 0x78: ALCMON, ALCCAL, ALCULOK and AUTOCAL enabled. Is that okay?

    I forgot to set those up in the screenshot.

    I can read and write from the LTC6951. At startup I read the registers and they match with default values. After writing they match with the ones written.

    Marta

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.