Post Go back to editing

AD9546 1Hz Output Duty Cycle Configuration

Thread Summary

The user wants to change the duty cycle for 1Hz outputs on the AD9546 EVB. The final answer explains that the Q divider value (Q0=1,225,500,000) and phase offset (0.8*2*1,225,500,000=1,960,800,000) must be configured using the Duty Cycle Adjust feature in the evaluation software. The registers 0x1108 to 0x1104 were updated to achieve the desired 80% duty cycle.
AI Generated Content
Category: Hardware
Product Number: AD9546

Hi, 

I have a system which contains AD9546 EVB.

I configured inputs and outputs and everything works fine. I am using an OCXO (10MHz) for reference.

But I want to change duty cycle for the all 1Hz outputs.

When I checked the datasheet, according to page 105, I understand that first I should get the "Q divider" value and make a calculation to get "Modulation Step". Then, I should write that values to the related registers.

However, when I read the value from registers of "Q Divider" using evaluation software, it returns hex "00". So I could not make the calculation.

Even If I tried to write random values to the register of both Q Divider and Modulation Step, nothing changed.

Is there any way to do that?

Thanks,