Post Go back to editing

Multi Chip Synchronization using AD9528

Category: Software
Product Number: AD9528
Software Version: Linux 14.04

Hi,

We are using three AD9528 in our configuation , where one A9528 is to synchronize other two .All three AD9528's are communicating over a single SPI protocal depending on their on Chip Select .

We are not able to observe the change in  sysref k- divider value , if we boot the FPGA by providing device clocks to the two AD9528's (other than controller AD9528) .

We are able to observe the device tree changes in the sysref frequency , if we disconnect device clocks to the two AD9528's and boot the board .

Can anyone help me out with this.

Thanks

Uma

Thread Notes

Parents
  • HI,

    I am not sure I have a clear picture of your system. If you could send me a block diagram of your system, it will help.

    You then say that when the FPGA changes sysref K-divider value, the AD9528 does not change the SYSREF clock. Is this what you are saying? Depending the SYSREF generation mode you use, you need to create a SYSREF request signal first. See the data sheet rev F, page 24 on how to create it.

    Petre 

  • Thanks for your reply,

    Here is overview of our system.

    Whenever I reboot the system , all devices ( ADRV9009's) are coming up and sysref clock frequency is 7.86MHz (Device clock / 16) . After running the profile config script for ADRV9009s, the sysref clock frequency automatically changed to 3.86MHz ( Device clk / 32).

    If I try rebooting the system by disconnecting the device clock form Top AD9528 to AD9528-1 ,we are getting sysref frequency as exactly what we expected.

    The thing I would like to highlight is that , in the same board we communicating with three AD9528's using single SPI ,depending on their Chip select as out enable.

     

  • Hi,

    I am afraid you need to open this issue on the ADRV9009 board. It seems you are using some scripts I am do not support

    Petre

Reply Children
No Data