Post Go back to editing

RF synthesizer with JESD204 support

Thread Summary

The user is seeking an RF PLL-based synthesizer with JESD204 SYSREF reclocking capabilities to meet the setup/hold timing constraints for a high-speed JESD204B converter (AD9162) clocked at up to 5 GHz. The ADF4378 was suggested, but it does not support differential swing lower than 1.0V for the 11 mm x 11 mm BGA package, making it incompatible with the AD9162 in this package. The user is looking for alternative solutions from Analog Devices that can drive the AD9162's SYSREF with the required differential swing.
AI Generated Content
Category: Hardware

Hello.

I am looking for RF synthesizer with JESD204 SYSREF reclocking feature. I attached the simplified schematic to clarify my task.

There is a Clock Synthesizer with JESD204B support (HMC7044 for example) which produces the Clock and SYSREF JESD204 signals.
The schematic also contains a High-Speed JESD204B converter (AD9162 for example) which should be clocked by a high frequency signal.
The clock frequency is up to 5 GHz ant it’s out of HMC7044 possibilities. One of the solutions is to use a RF PLL-based Synthesizer.
But most of High-Speed JESD204B devises (which are Subclass 1 compliant) has strong constraints for Setup/Hold timings between the Clock and SYSREF signals.
So I am looking for RF PLL-based synthesizer which will produce high-frequency output clock and will be able to reclock the SYSREF input signal
by output clock in order to have predictable timings. I think that without reclocking it can be some timing uncertainty with the temperature / power supply changes
and power On/Off cycles (because of desynchronization  of internal PLL dividers).
I know the Texas Instruments' LMX2594 device with appropriate features but it has some limitations regarding to values of PLL dividers (in SYSREF mode) and does not meet my requirements.
My question is which solutions are possible with Analog Devices products for such application?

P.S. The AD9213 High-Speed JESD204 ADC has useful "Averaged SYSREF" mode which eliminates the SYSREF Setup/Hold timing constraints,
but unfortunately most of JESD204-compliant devices has no such feature.

Regards, Boris.

Edit Notes

Minor updates
[edited by: BorisBree at 1:30 PM (GMT -5) on 28 Nov 2023]
Parents
  • Hi, Boris,

    I knew you connected with Chris about your query.

    For community reference, I am attaching our one of the latest PLL/VCO synthesizer datasheet. ADF4378 is 12.8GHz frequency synthezier with an additional general purpose pulse retimer feature.
    Link to product page: www.analog.com/.../ADF4378.html

    Feel free to create an EZ thread if you have a question.

    Thanks,
    Emrecan

  • Hi, Emrecan.

    Thank you very much for this information. 

    ADF4378 is an interesting device with perfect phase noise performance. It fits my requirements at all, except for one point. I need a device what will generate a reclocked SYSREF for AD9162 DAC in 11 mm × 11 mm BGA package (there are 2 BGA packages exists for it). But 11 mm x 11 mm package does not support SYSREF differential swing lower than 1.0V. I have discussed it in this thread:  https://ez.analog.com/data_converters/high-speed_dacs/f/q-a/576128/ad9162bbcaz-sysref-differential-swing
    According to Datasheet, the ADF4378 has SYSREF Output Differential Voltage = 0.85V. And I have not found information that Output Differential Voltage can be programmed for higher levels. So, it seems that ADF4378 cannot drive SYSREF for AD9162 in 11 mm × 11 mm package.
    Unfortunately I can not choose the  AD9162 in 8 mm × 8 mm BGA package due to limitations of our manufacturing process (the distance between balls and the balls itself are too small).
    It's a pity that two devices from the same manufacturer are incompatible  :)

    In any case, thank you for information. I hope I can try ADF4378 in future projects. The device is really good.


Reply
  • Hi, Emrecan.

    Thank you very much for this information. 

    ADF4378 is an interesting device with perfect phase noise performance. It fits my requirements at all, except for one point. I need a device what will generate a reclocked SYSREF for AD9162 DAC in 11 mm × 11 mm BGA package (there are 2 BGA packages exists for it). But 11 mm x 11 mm package does not support SYSREF differential swing lower than 1.0V. I have discussed it in this thread:  https://ez.analog.com/data_converters/high-speed_dacs/f/q-a/576128/ad9162bbcaz-sysref-differential-swing
    According to Datasheet, the ADF4378 has SYSREF Output Differential Voltage = 0.85V. And I have not found information that Output Differential Voltage can be programmed for higher levels. So, it seems that ADF4378 cannot drive SYSREF for AD9162 in 11 mm × 11 mm package.
    Unfortunately I can not choose the  AD9162 in 8 mm × 8 mm BGA package due to limitations of our manufacturing process (the distance between balls and the balls itself are too small).
    It's a pity that two devices from the same manufacturer are incompatible  :)

    In any case, thank you for information. I hope I can try ADF4378 in future projects. The device is really good.


Children
No Data