Post Go back to editing

AD9547 Clock Configuration File

Thread Summary

The user requested configuration files for the AD9547 to generate output clocks of 155.52 MHz and 13.824 MHz, synchronized to an external reference clock of 1 kHz or 2 kHz. The support engineer provided a configuration file for 13.824 MHz and suggested using a 25 MHz XO as the SYSCLK input. The user also shared schematics, which were reviewed and found to be mostly correct, with a few minor adjustments recommended. The user later requested updated configuration files for 13.312 MHz and 61.44 MHz outputs.
AI Generated Content
Category: Software
Product Number: AD9547

Hi ADI Team,

We are planning to use AD9547BCPZ as our clock sync. As I am new to this IC could you please help me with the clock configuration file for this IC.

1. Profile 1: Output Freq 155.52MHz
2. Profile 2: Output Freq 13.824MHz

Please also suggest the Input XO frequency that we can proceed with.

We need to synchronize these output clocks with an external clock frequency of 1PPS or 2KHz.