Post Go back to editing

How to program EEPROM on the AD9546 eval board?

Category: Software
Product Number: AD9546

Hi,

I am working on the AD9546 Evaluation Software (Rev. 1.3.0.0) to configure my AD9546 Eval Board and I want to load my configuration into the EEPROM on the board. 

On Evaluation Software there is an EEPROM tab to set somethings there. But in the user guide it says "This window cannot be used with the AD9546 evaluation board because the board does not contain a EEPROM usable to store the AD9546 configuration." But on the schematics there is an EEPROM.

On the other hand I also have Evaluation Board USB Flash Programmer and when I select the board and .iic file, I can load something to the EEPROM.

So, could you please tell me how can I generate .iic file which consists my config from the Evaluation Software?

Thanks,