Post Go back to editing

HMC7044 Register set

Category: Hardware
Product Number: HMC7044

Hi,

I am try to extract register set for HMC7044,ADI rep provided the .clk file only.

How to get get required register configuration set for hmc7044?

Please provide register set for below configuration.

HMC7044 Input Clock : 137 MHz

 

Output Ports

Required clock Frequency

CLKOUT2  -Sample Clock 

137 MHz

 

SCLKOUT3  -SYSREF 

4.28 MHz

 

CLKOUT12  -FPGA Ref clock

137 MHz

 

SCLKOUT13  -SYSREF 

4.28 MHz

 

Thanks In Advance.

VK19

  • ADI North America will be on summer shutdown starting August 24, 2023; perhaps another community member can assist you until our return on September 5th.
  • Hi VK19,

    You can use HMC7044 evaluation software to extract your register values. You can download evaluation software from the below link.

    Link: EVAL-HMC7044 Evaluation Board | Analog Devices

    You can use this software to set your input buffer settings, PLL1 and PLL2 configuration as well as the output network configurations. There are a couple of important points when using GUI,

    1- You need to update the below registers,

    2- SYSREF timer value should be integer multiple of channel divider values. 

    3- I recommend setting output driver mode to LVPECL for SYSREF channels if you are using pulsed SYSREF as LVDS has problems with keeping logic 0 state at idle when using LVDS. This is not valid for continuous signals and SYSREFs. You can create a level translator circuit for the LVPECL-LVDS interface. 

    As a side note, the minimum external VCO input frequency is 400MHz. If you are using 137MHz without using the internal VCO of HMC7044 (which means HMC7044 is in clock distribution mode), HMC7044 will not work as expected. If you are using PLL1 and PLL2 or just PLL2, you can use a 137MHz signal as a reference. 

    I cannot create a register set file without knowing your project requirements and design. I recommend checking the evaluation software of HMC7044 to create the register settings for HMC7044. If you have any questions later on, feel free to reach out. You can share your ADISimCLK file and design requirements as well as your evaluation software output. 

  • Thank you so much for your reply,

    external reference clock is not a problem for me ,anything is fine but output clock requirement as mentioned above.

    while uploading .clk file it is showing some file format error, so i have changed file format .

    Please find it below ,internal pll selection also anything is fine.

    Thanks

    VK19

    HMC7044_CLK_Config.txt

  • Hi VK19,

    According to your ADISimCLK file, you are using both PLL1 and PLL2. I attached a typical HMC7044 configuration for dual pll operation with your ADISimCLK configuration. You can see PLL1 and PLL2 configurations and output channel configuration, for other details you can check the datasheet. Below register settings are for typical applications. Your requirements may be different.

     DUAL_PLL_137MHZ_VCXO_137MHz_OUT.zip

    Thanks,

    Emrecan