HI
I am planning to have clock tree structure using LTC6952(Clock +SYSREF) as source and LTC6955(1Nos for Clock and 1Nos for SYSREF) as fan out followers.
Kindly confirm if all the outputs of LTC6955 can be phase aligned.
Thanks in-advance,
Deva
LTC6952
Last Time Buy
The LTC6952 is a high performance, ultralow jitter,
JESD204B/C clock generation and distribution IC. It
includes a Phase Locked Loop (PLL) core, consisting...
Datasheet
LTC6952 on Analog.com
LTC6955
Last Time Buy
The LTC6955 is a high performance, ultralow jitter,
fanout clock buffer with eleven outputs. Its 4-pin parallel
control port allows for multiple output...
Datasheet
LTC6955 on Analog.com
LTC6953
Last Time Buy
The LTC6953 is a high performance, ultralow jitter, JESD204B/C clock distribution IC. The LTC6953’s eleven outputs can be configured as up to five JESD204B...
Datasheet
LTC6953 on Analog.com
HI
I am planning to have clock tree structure using LTC6952(Clock +SYSREF) as source and LTC6955(1Nos for Clock and 1Nos for SYSREF) as fan out followers.
Kindly confirm if all the outputs of LTC6955 can be phase aligned.
Thanks in-advance,
Deva
Hi Deva1998
Since LTC6955 is a simple buffer, it doesn't support EZSync or ParallelSync applications. However, as the divider value is 1, the phase of the outputs will not change over time or after power up except OUT10.
You can assume the skew between channels is in the limits of the below table.

However, if you want to distribute SYSREF signal, It is important that SYSREF signals can be delayed individually according to the layout need. Therefore, I recommend using LTC6952 and LTC6953 in order to create a clocking tree.
Thanks,
Emrecan
Hi Deva1998
Since LTC6955 is a simple buffer, it doesn't support EZSync or ParallelSync applications. However, as the divider value is 1, the phase of the outputs will not change over time or after power up except OUT10.
You can assume the skew between channels is in the limits of the below table.

However, if you want to distribute SYSREF signal, It is important that SYSREF signals can be delayed individually according to the layout need. Therefore, I recommend using LTC6952 and LTC6953 in order to create a clocking tree.
Thanks,
Emrecan
Hi,
Thank you for your suggestion. in ltc6955 the out10 is not a divider output but it is said that phase of all outputs will not change except out10. Kindly reconfirm the same.