Post Go back to editing

Clock Generator for AD9680-LF1000EBZ evaluation board and FPGA Development Board

Thread Summary

The user is planning to purchase an AD9680-LF1000EBZ evaluation board and wants to know if the onboard clock generator is sufficient for interfacing with a third-party FPGA development board for DSP on the JESD204B interface. The final answer suggests that the AD9528 and HMC7044 can generate the required DEVCLK and SYSREF signals, but recommends posting the question on the High Speed ADCs forum for a more precise recommendation. The user confirms they will post on the recommended forum.
AI Generated Content
Category: Hardware
Product Number: AD9680-LF1000EBZ

Hi,
We are planning to purchase an AD9680-LF1000EBZ evaluation board which is to be interfaced with our third-party FPGA development board. My question is: whether the onboard clock generator of the AD9680-LF1000EBZ evaluation board is sufficient for all the required clock signals (Like sample and reference clock for ADC and clocks for FPGA) to carry out DSP on the JESD204B interface using the above boards. or is an additional clock evaluation board needed? If yes then, please suggest a suitable and economical model of it. I explored the ADI website and found the following clock evaluation boards but not sure which one is the most suitable one. These boards are AD9525, AD 9528, AD9526-0, and HMC 7044. Please help. Thanks.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.