Post Go back to editing

DS3231M What is the definition of a I2C Inactive for battery mode.

Thread Summary

The user inquires about the DS3231 RTC's lowest current consumption mode, specifically if the I2C interface is considered inactive when unpowered and the SCL/SDA pins are low. The final answer confirms that I2C inactive means not sending or receiving data, and the DS3231's timekeeping battery current is typically 0.8uA, with a maximum of 3uA. The accompanying answer clarifies that the DS3231M has a different current consumption of 2uA.
AI Generated Content
Category: Datasheet/Specs
Product Number: DS3231M
Software Version: Not Applicable

Hi,

I have a question about specifications. To have the DS3231 RTC in the lowest current consumption mode it must run on battery with its I2c inactive, see  Maxim Integrated page 3 section VBAT Current Consumption. The definition of what an inactive I2C interface is is not clear specified in the specifications.

I use the chip as a watch dog to periodic power up a system using its Int/SQW open collector output activating a Pmosfet which acts as a switch to the system to be power up. In a power off mode the  DS3231 I2C interfaces is unpowered and down/low including, the RTC chip receives only power using a battery. Is in this state, the I2C considered inactive and so the current consumption 2uA.?

Is the definition of an inactive I2c interface in this specification one with inactive not changing SCL and SDA pins independent of the voltage levels high or low at these pins, in my case active low because of the lac of VCC at the microcontroller.

Hope someone can clear this up.

Thanks

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.