Post Go back to editing

Technical support for ADCLK946

Thread Summary

The user inquired about the minimum and maximum input frequency for the ADCLK946 in both single-ended and differential modes. The final answer stated that the maximum input frequency is 4.5GHz to 4.8GHz, applicable to both modes, while the minimum input frequency was not characterized for this part.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADCLK946

Hi,

What is the Minimum and maximum input frequency that can be given to ADCLK946 in both single-ended and differential Mode?

  • Hi,

    The maximum output frequency that the ADCLK946 can produce ranges from 4.5GHz to 4.8GHz. With this, the maximum input frequency that can be given to the part is from 4.5GHz to 4.8GHz. This value applies for both single-ended and differential mode. On the other hand, the minimum input frequency was not characterized for this part.

    Best regards,
    Mark

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.