Post Go back to editing

AD9517-3 OUTPUTS just lasting for 30ms

Thread Summary

The user is experiencing an issue with the AD9517-3 internal VCO, where the generated clock only lasts for 30ms. The support engineer requested the STP file used for configuration and details on the configuration procedure post-power-up, to diagnose the problem further.
AI Generated Content
Category: Hardware
Product Number: AD9517
Software Version: KEIL5

We are using the internal VCO of AD9517-3 to generating clks. But we can only generate a clock which lasting for 30ms. 

We can change the freqency of the output.