We are using AD9517-3 for clk generation. Until now we have successfully used OU0/OUT1 for LVPECL and OUT5 for LVDS&CMOS.
But we can't use OUT2&OU3,OUT4&OUT6&OUT7 for clk distribution.
The value of registers are referred to evaluation software and the registers map:
"Addr(Hex)","Value(Bin)","Value(Hex)"
"0000","00011000","99"
"0001","00000000","00"
"0002","00010000","10"
"0003","01010011","53"
"0004","00000000","00"
"0010","01111101","7D"
"0011","00000001","01"
"0012","00000000","00"
"0013","00000000","00"
"0014","00000011","03"
"0015","00000000","00"
"0016","00000110","06"
"0017","00000000","00"
"0018","00000111","07"
"0019","00000000","00"
"001A","00000000","00"
"001B","00000000","00"
"001C","00000000","00"
"001D","00000000","00"
"001E","00000000","00"
"001F","00001110","0E"
"00A0","00000000","00"
"00A1","00000000","00"
"00A2","00000000","00"
"00A3","00000000","00"
"00A4","00000000","00"
"00A5","00000000","00"
"00A6","00000001","01"
"00A7","00000000","00"
"00A8","00000000","00"
"00A9","00000001","01"
"00AA","00000000","00"
"00AB","00000000","00"
"00F0","00001000","08"
"00F1","00001010","0A"
"00F4","00001000","08"
"00F5","00001000","08"
"0140","01000010","42"
"0141","01011010","5A"
"0142","01000010","42"
"0143","01000010","42"
"0190","00010001","11"
"0191","00000000","00"
"0192","00000000","00"
"0196","00000000","00"
"0197","10000000","80"
"0198","00000000","00"
"0199","00000000","00"
"019A","00000000","00"
"019B","00100010","22"
"019C","00000000","00"
"019D","00000000","00"
"019E","00010001","11"
"019F","00000000","00"
"01A0","00010001","11"
"01A1","00000000","00"
"01A2","00000000","00"
"01A3","00000000","00"
"01E0","00000101","05"
"01E1","00000001","01"
"0230","00000000","00"
"0231","00000000","00"
"0232","00000000","00"
Is there any erro? Thanks.