AD9542
Recommended for New Designs
The 10 clock outputs of the AD9542 are synchronized to any one of up to four input references. The digital phase-locked loops (DPLLs) reduce timing jitter...
Datasheet
AD9542 on Analog.com
AD9545
Recommended for New Designs
The AD9545 supports existing and emerging International Telecommunications Union (ITU) standards for the delivery of frequency, phase, and time of day...
Datasheet
AD9545 on Analog.com
Hi,
I have an external 10,000 Hz reference signal connected to REFBB on an AD9542 but I'm having trouble getting it non-fault lock.
The reference signal has a nominal tolerance of 600 ppm which I interpret as the signal can be anywhere from 9,994 to 10,006 Hz.
According to my calculations, I think this yields a delta p of 599640 ppb [from the formula -600E-6/(1+600E-6)*1E9= -599640.2159]
This is what is programmed into the ΔTOL register for REFBB [0x092658].
IS THIS CORRECT?
In my current rig, the actual reference input is measured at 10,003 Hz (and it's not easy for me to change this) and I can not get a valid reference lock: REFBB status (0x3008) only ever reports 'fast' and 'fault'. The register is working as it reports 'los' (and sometimes both fast and slow) when the signal is removed.
I believe that the 52 MHz chip reference oscillator is good as I am able to synthesize a 10,000.00 Hz signal on the outputs.
Any suggestions greatly appreciated.
Thanks,
Steve