Hi,
I have two problems.
1. I could not connect AD9545 through ACE version 1.27.3250.1427.
It didn't attach the hardware even through I "refresh Attached Hardware".
2. Using ACE 1.10.2671.1118, I could connect AD9545 Eval. board as follows.( But it displayed " Unapproved" mark.)
After setting the several parameters in the configuration wizard, I applied it using "Apply" button and " Apply changes".
Also I turn on "Auto Apply" and I can see the "successful" log as follows.
But when I "read All", parameters were not the same what I applied in the previous step.
In the following figure, all outputs are set to "Zero". I wanted to turn on OUT0A.
How can I solve these problems ?
Thanks in advance.
Best regards,
Olive.