Post Go back to editing

ADN2915 recover clock full rate output can reach 10GHz?

Thread Summary

The user inquires about using the ADN2915 to recover a 10GHz clock from a 10Gbps data rate without outputting the data. The final answer suggests referring to page 18 of the ADN2915 datasheet, which shows that setting OUTPUTA.D2 to 1 (DDR clock disabled) will achieve the desired clock recovery without data output.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADN2915

My data rate is 10Gbps,and I want to output recover clock which is 10GHz(SDR) ,meanwhile I don't want the output data,I only need the recover clock.

Can I use the register OUTPUTA.D2=1 (DDR clock disabled) ?

From Figure 1 : BLOCK DIAGRAM ,if close the DDR function ,I would achieve goal.

Thanks!

Parents Reply Children
No Data