Hi,
As shown in the picture below, I use a 122.88MHz VCXO for PLL1. But my signal generator only gives a reference clock of 100MHz so I use that 100MHz reference clock for the HMC7044. My problem is that the PLL1 did not lock. I configure the PLL1 as below:
1. CLKIN0 Prescaler = 2 (0x001C = 0x02)
2. N1 divider = 1536 (0x0027 = 06, 0x0026 = 00)
3. R1 divider = 625 (0x0022 = 02, 0x0021 = 71)
4. Timer threshold = 31 (0x0028 = 0x1F)
for this configuration, the PD1 frequency was 80 kHz (Was it too small?). I check the PLL1 status register (0x007C) it switches between 0x4E and 0xCE. that means the PLL1 is near lock but it never locks. Can you help me out with this problem?
Thank you in advance.