Post Go back to editing

How to choose a high-performance clock device?

Thread Summary

The user seeks a 5-channel 400MHz clock with -130dBc/Hz phase noise at 1kHz offset. The HMC7044 cannot meet this requirement due to its 1/f noise. The LTC6952, with a 1/f FOM of -281 dBc, can achieve -139 dBc at 1kHz offset, provided a 100 MHz reference oscillator with -145 dBc phase noise at 1kHz is used. The VCO noise within the loop bandwidth is suppressed by the loop filter, so the LTC6948 is recommended as an external VCO for the LTC6952.
AI Generated Content
Category: Hardware
Product Number: HMC7044
Software Version: HMC7044

hello!

I want to output a 5-channel 400MHz high-performance clock, and the phase noise of the clock can reach -130dBc@1kHz. Do you have a good clock solution?

I used the ADIsimclk evaluation tool to evaluate the HMC7044 and found that the -130dBc@1kHz specification could not be met.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.