Post Go back to editing

How to choose a high-performance clock device?

Thread Summary

The user seeks a 5-channel 400MHz clock with -130dBc/Hz phase noise at 1kHz offset. The HMC7044 cannot meet this requirement due to its 1/f noise. The LTC6952, with a 1/f FOM of -281 dBc, can achieve -139 dBc at 1kHz offset, provided a 100 MHz reference oscillator with -145 dBc phase noise at 1kHz is used. The VCO noise within the loop bandwidth is suppressed by the loop filter, so the LTC6948 is recommended as an external VCO for the LTC6952.
AI Generated Content
Category: Hardware
Product Number: HMC7044
Software Version: HMC7044

hello!

I want to output a 5-channel 400MHz high-performance clock, and the phase noise of the clock can reach -130dBc@1kHz. Do you have a good clock solution?

I used the ADIsimclk evaluation tool to evaluate the HMC7044 and found that the -130dBc@1kHz specification could not be met.

Parents
  • Hi,

    Phase noise value at 1kHz offset will be completely dependent on 1/f noise of the PLL and the reference source noise. If we ignore the noise coming from the reference and only encounter 1/f noise of the PLL, you need to find a part that has 1/f noise at least -272dBc/Hz (not normalized) according to the formula: 

    PN_1kHz = FOM_1f + 20*log10(fout) - 10* log10(f_offset)

    -130 = FOM_1f + 20*log10(400 x 10^6) - 10*log10(10^3)   ---->   FOM_1f = -272 dBc 

    1/f FOM of HMC7044 is -252 which clearly shows that this spec cannot be met with HMC7044. 

    LTC6952 has 1/f FOM of -281 dBc and the corresponding 1/f noise for 400 MHz output at 1 kHz offset will be ~ -139 dBc. So, it can provide good margin. 

    Now, you have to consider the noise coming from the reference. Reference noise will translate with 20* log10(fout/fref) relation (let's assume you are using 100 MHz reference clock), meaning that the noise contribution of the reference will be 12 dB higher than the value that you are given in the reference oscillator datasheet. Your aim is to get -130 dBc at 1kHz, so you have to find a 100 MHz crystal oscillator that has a PN value of -142 dBc at 1 kHz. (Note that 1/f noise contribution is ignored as the total noise will be dominated by the reference, the 1/f noise contribution might be considered as negligible here.) With a few dB margin, you need to aim a crystal that has ~-145 dBc PN at 1kHz offset. 

    CCSS-945-100 crystal oscillator from Crystek is a good crsytal oscillator which can achieve this goal. Datasheet link is below. 

    CCSS-945.pdf (crystek.com)

    The only remaining thing is to find an external VCO that works within the range of LTC6952 because LTC6952 does not have an internal VCO. 

    Regards,

    Kudret

  • Hi ,  Kudret

    Thank you for the reply!

Reply Children
No Data