Hello.
Is there any way to mute or power down the AD9528 clock outputs without also powering down the output divider? I have found that the output dividers lose their phase relationship if I use the channel power down registers 0x0501 or 0x0502 to disable and then enable an output.
Ideally, I would like the outputs to maintain their phase relationship when the outputs are turned off then on and I do not want to resync the dividers afterwards.
So if there is a register that can just turn off the output buffer that would be ideal!
Thanks for the help.