Post Go back to editing

Output shape issue with AD9542

Category: Software
Product Number: AD9542

Issue with creating clean 122.88 MHz clock signal using AD9542. Using valid 10 MHz ref input. I have attached cso file, screenshots of o'scope and of ACE software. In ACE, the mux in DPLL0 and DPLL1 is highlighted red, not sure where that error is coming from. I am using the AD9542 eval board. Spectrum analyzer signal output is just as bad, with many harmonics. Would appreciate any help.  The CSO file had issues uploading, had to send as a txt file. Thanks, Alex

ses122p88txt.txt