Post Go back to editing

AD9542 Eval Board I2C jumper settings

Category: Hardware
Product Number: AD9542

Hi Petre,

I am trying to communicate with the AD9542 on the eval board using an external I2C master. However, I'm confused by the table in the wiki which appears to be in conflict with the schematic:

I feel for I2C operation, I should be making P605 1-2 / 5-6 / 8-9 to match Table 68. Is the wiki incorrect? I checked on AD9544 and AD9545 which seems to be the same.

I have removed P506, P507 and P508 and I'm connecting the external I2C master via P512. Anything else to do?

Thanks, Steve

Parents Reply Children
No Data