Post Go back to editing

Feasibility of double input Reference on LTC6954

I have double reference sources available on my system, but just one is ON in the operating condition.

The Reference sources are two LVCMOS square clock at 100 MHz. At any time, when the first one is ON the other is OFF, and viceversa.

I adopted the LTC6954-4 as Reference buffer, can I connect the the IN+ input to the first one Reference source and the IN- input for the second source?

In case of yess, which is the correct scheamatic layout for this solution?

Thank you in advance for the reply.