Hi,
I want to ask question about ADCLK854's jitter. I use AD9528 to give ADCLK854 320 MHz. In the datasheet Table 2. There are some jitter in the same bank and all outputs are LVDS's situation. My questions as below:
1.If I have 50+65 ps jitter when all of my outputs are LVDS or just 65 ps because they are in the same part, even in the different bank?
2. In the different bank, can I expect all jitter are the same? Or it will be different in different banks because the 50 ps and 65 ps are maximum value, so it maybe will be 10, 25 and 40 ps in different bank? If the answer is yes, it will effect the output waveforms if I want them to send 320 MHz at the same time, right?
Correct me if I am wrong.
Many thanks.
Mike