Hi,
I am using AD9528 clock module to generate a clock for the FPGA and ADRV.
The clock which i was able to generate was 2-SYSREF-120Khz and 2-DEVCLK-245.76MHz .
i also want to 100MHz clock output which i am not able to generate. I was able to get 100.53MHz clock but that would alter my other clock frequency's.
Setup file is also attached along with the picture.
Input i have given:
REFA:122.88MHZ.
REFB:0MHz
SYSREF:0MHz
CLK IN:122.88MHz
OUTPUT REQUIRED:
OUT1 : 120KHz.
OUT2 : 120KHz
OUT3 : 245.76MHz
OUT4 : 245.76MHZ
OUT5 : 100MHz