All,
Trying to buffer a 10Mhz sine wave to a 10Mhz 3V3 square wave. The LTC6957-3 seemed ideal to me.
I have been trying to use the EVK board "DC1766A" to generate the required output. But so far I am only getting a pk-pk of 600mV, half of it can be accounted for because of the EVK boards output.
"AC coupled and attenuated through two 100Ω resistors as shown in the DC1766A schematic diagram to present a 50Ω source impedance appropriate to connect to a 50Ω input impedance instrument."
But I would expect 1.65V to appear at my output in this case and not the 600mV im seeing at the moment.
Input single-ended 10Mhz 1v pk-pk sine
V+ = Vdd = 3v3