Post Go back to editing

Reg: ADF4355 frequency lock

Hi Sir, 

I have a problem with frequency locking in ADF4355. When I'm writing values on registers based on the  4355 evaluation software GUI, I'm not able to lock the exact frequency.

My frequency is deviating to some other value. when I'm locking the frequency at 212.5MHz  it is giving output as 298MHz.

Please find the register values below.

Rego  : 0x002002A0

Reg1 : 0x08000001

Reg2 : 0x00000012

Reg3 :0x40000003

Reg4 :0x32008984

Reg5 :0x00800025

Reg6: 0x348480F6

Reg7:0x100002E7

Reg8:0x102D0428

Reg9:0x01034399

Reg10:0x00C001FA

Reg11:0x0061300B

Reg12:0x00 61300B

Parents Reply Children
No Data