Hi
I have a few questions about the reference clock of HMC7044, and how to configure it.
1- Can I use the OH300-71003SV-100.0M oscillator with 100MHz sine output and 5 dBm amplitude for the second PLL via PIN OSCIN like the photo below?
2- Can I use the CPOUT1 pin from the HMC7044 to control the oscillator control voltage pin, is the output voltage of CPOUT1 suitable for the oscillator control voltage pin?
3- Is the oscillator output configuration suitable for the HMC7044 OSCIN pin?
http://www.conwin.com/datasheets/cx/cx282.pdf
Thank you in advance.