ADCLK944/946 - DC-coupled single ended inputs

Hello,

the datasheet of the ADCLK944 and ADCLK946 states that they are able to handle single ended DC-coupled input signals. In the datasheet under the "input termination options" section (page 11 of Rev. B datasheet) there is no figure that showes how to interface with a single ended DC-coupled input signal.

In the datasheet of the ADCLK948 i found the following figure:

I interpret this figure as follows:Vref and Vt left floating, single ended DC-coupled input signal connected directly to CLK and /CLK connected to GND via a series capacitor.

Can i assume that this input termination for single ended DC-coupled input signals also apply for the ADCLK944/946? If not, can you provide me with some information on how to interface with a single ended DC-coupled input signal when using the ADCLK944/946?

Thank you in advance.

Kind regards,

Lukas

Parents Reply Children